8/30/2013 8:20 AM | |
Posts: 46 Rating: (4) |
Yes, I might have been a bit unclear about that. After I installed the GSD file, i added the IM151 module from the catalog. But now it appears as a unassigned device in the Project tree "Device", and I'm no sure if i can program it the same way as if I added at an ET200S with the corresponding IM151 module. I attached a picture of my network view and my project tree. Attachmentscreenshots.zip (365 Downloads) |
8/30/2013 9:08 AM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168) |
Hello, When you click on "not assigned", can you select the desired CPU? Best regards, Wizard |
8/30/2013 9:38 AM | |
Posts: 46 Rating: (4) |
When i click the "not assigned" link in network view, nothing happens. I tried opening up a new project in TIA v11 and create a new device, but it is not available there either. According to this documenthttp://www.automatyka.siemens.pl/docs/docs_ia/st70_2013_9_ET200.pdfthe IM151-3 PN is listed as "Interface module without CPU"? Edit: I could rightclick the "not assigned" link, and add IO controller. But the 1215CPU was the only one available.. |
Last edited by: MatsNil at: 8/30/2013 9:43 AM |
|
9/3/2013 1:05 PM | |
Posts: 46 Rating: (4) |
I ended up connecting it to the 1215CPU. |
Follow us on