1/12/2018 2:55 PM | |
Joined: 10/16/2007 Last visit: 5/3/2023 Posts: 599 Rating:
|
Hello, check the Profibus-adress adjusted on the ET200S and also the wiring of the Profibus-plugs. Regards |
1/12/2018 3:59 PM | |
Posts: 17 Rating:
|
Hi, I have already checked it , and it is ok ! I have a question ; Should I define on HW config which terminal module TM I'm using ? Regards |
1/17/2018 4:00 PM | |
Posts: 17 Rating:
|
Thank you for help. I did that, but I still have the error. |
1/17/2018 10:06 PM | |
Joined: 1/21/2013 Last visit: 4/21/2023 Posts: 4617 Rating:
|
Hello, still BF flashing? |
1/17/2018 10:09 PM | |
Posts: 17 Rating:
|
Yes It still flashing and on SF solid red |
1/17/2018 10:11 PM | |
Joined: 1/21/2013 Last visit: 4/21/2023 Posts: 4617 Rating:
|
Also on the ET200S BF flashing? |
1/17/2018 10:22 PM | |
Posts: 17 Rating:
|
The BF on ET 200S and the BF of CPU are flashing. It gives me on the diagnostic of slave : Error modul on slot 1 and No modul on slot 2 to 13 |
Follow us on