1/12/2018 12:18 AM | |
Posts: 36 Rating: (1) |
I have a question concerning wiring of ET200SP https://support.industry.siemens.com/cs/ww/en/view/59753552 On the page nr 15 there is example of 1-wire and 2-wire connection. What are the differences between connecting sensor in those two ways? I mean what are advantages and disadvantages of each of those two solutions? L+ is an external power supply delivered via backplane to et200 module. what about 24VDC? it is produced by et200? If i wired for example following pairs: 2,10 ; 3; 4,12; 6,14; 8,16 i would obtain more diagnostic features? If I break L+ wire, they will also fail, because module will be not capable of producing +24VDC anymore? I am sorry for this simple question but maybe i don't understand some very basic concept. |
Last edited by: Jen_Moderator at: 1/15/2018 11:34:47 AMInserted right link. |
|