6/1/2010 2:01 PM | |
Posts: 4 Rating: (0) |
5x 315-2 PN/DP using FB63-TSEND, FB64-TRCV, FB65-TCON, FB66-TDISCON |
6/1/2010 2:38 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, This is because of using OB100 (this is a restart OB and is run when the CPU is restarted (warm start)). In this OB, the first communication trigger is enabled with marker 0.3 "START-UP".This bit after that start let's say "communication". In case if you build connection like this FAQ http://support.automation.siemens.com/WW/view/en/29737950 Am I right? Best regards, Hristo Mihalev |
6/2/2010 8:49 AM | |
Posts: 4 Rating: (0) |
yes run with other cables. 200m maybe. |
Follow us on