1/23/2019 12:48 PM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Thank You! Technology Team, We have one machine where attached baumer encoder are installed, now these encoders are obsoleted, so we want to replace these with new SIEMENS absolute encoder on existing S7-300 Hardware. The old one (baumer) having configuration PNO-Class 2 16Bit resolution with Length of one IQ Words. The new one (SIEMENS) having Class 1&2 Single Turn with Length of one IQ Words. and as well Class 1&2 Multi Turn with Length of two IQ Words. If you can share sample FC/FB for Absolute Encoder 6FX2001-5QP24 it will be supported to integrate in existing scenario. Attachmentatd3bb14y13(profibus-dp).pdf (539 Downloads) |
MS |
|
6/15/2019 4:48 PM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
AttachmentAbsolute Encoder Example.zip (800 Downloads) |
MS |
|
This contribution was helpful to1 thankful Users |
Follow us on