5/8/2011 4:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Perhpas there you will find an answer- http://support.automation.siemens.com/WW/view/en/837001 http://support.automation.siemens.com/WW/view/en/18645578 Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/8/2011 4:54 PM |
|
5/11/2011 11:33 AM | |
Posts: 204 Rating: (1) |
Thanks for yours help, I found what I need |
5/24/2011 12:20 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359) |
Hi Cells in a datablock can be considered as 1- The read only cells in which, you only read the data.These are possibly the constant or some scientific coeficient which is used in calculation.They are initialized and the values be unchanged for a long time. 2-The other cells, the CPU can write in them and they may change simply after you downlad the project.It is always a matter of problem.In process with adaptive parameters or process with lots of modification of setpoints and controllers' parameters, it is recommended to update the finalized DB values after finishing commissioning or before downloading the raw and original program.This is an important fact "The machine or process stabilized by the Values of datablock inside the CPU". Also check the following post: Datablock backup
Regards |
Follow us on