Industry Online Support
Technical Forum
9/22/2017 9:41 PM | |
Posts: 2 Rating: (0) |
I'm using the data logging to a S7-1200,I have an HMI that inputs parameters as a string, that data is sent to a data structure in a database. When I push a button on the HMI the structure is written to a local file as a .csv that can be downloaded via the web GUI. All of this works. What my problem is the data fields in the CSV have many extra spaces after the data input. I have checked that spaces are not in the data using the LEN command. I have linked to a zip of the project and a sample .csv. Software: Step 7 Basic Version 13 update 9 Link: Program and CSV - https://goo.gl/BNQ36U |
Last edited by: amartin16 at: 9/22/2017 9:42:52 PMLast edited by: amartin16 at: 9/22/2017 9:44:33 PM |
|
Follow us on