Industry Online Support
Technical Forum
11/20/2018 8:50 PM | |
Joined: 2/17/2014 Last visit: 9/13/2024 Posts: 6 Rating: (0) |
Dear Sir, We have S7 412-5H PN/DP CPU with ET200M Remote Racks over Profibus. Remote IO modules are of mixed type (Standard & Failsafe). We have Failsafe Modules as- AI Module (6ES& 336-4GE00-0AB0), F-DI Namur Module (6ES7 326-1RF01-0AB0) and F-DO Module (6ES7 326-2BF41-0AB0). We have activated Failsafe mode in CPU Properties and also assigned the DIP switch setting as per the HWCFG and everything is healthy. Now, we would like to program for these modules so that we can read values coming at them from field using CFC. We are working first time on Failsafe system, kindly help us to program these modules. we tried using F_CH_AI, F_CH_DI & F_CH_DO FBs but to no avail. Kindly help us to solve this issue, If possible kindly send us the Program for one channel from each Module. Please find enclosed Hwcfg file for the same. We shall be grateful for your kind support. Thanks.
AttachmentLCP-1001.zip (190 Downloads) |
Follow us on