9/13/2021 6:29 AM | |
Joined: 1/25/2020 Last visit: 3/19/2023 Posts: 12 Rating: (0) |
Hi These are normal induction motors. When there is no start command to the drive , even then this current is observed. |
9/16/2021 8:15 PM | |
Joined: 1/25/2020 Last visit: 3/19/2023 Posts: 12 Rating: (0) |
Yes, you are correct. |
9/17/2021 6:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Which is drive? Which is CU? Is earthing/ground connection of drive & motor is as per Siemens recommendations? |
6/5/2022 6:16 AM | |
Joined: 1/25/2020 Last visit: 3/19/2023 Posts: 12 Rating: (0) |
Hello Can any drive expert support ? |
6/7/2022 6:32 AM | |
Joined: 1/25/2020 Last visit: 3/19/2023 Posts: 12 Rating: (0) |
Hi Its Fluke 375. We check current in each phase one at a time. |
Follow us on