Industry Online Support
Technical Forum
8/30/2011 2:26 PM | |
Posts: 3 Rating: (0) |
Thank youwatr_fallr. But, can you give me one example of a device whose input to the controller is so fast that it will require such a narrow debouncing filter of 0.2msec or even 0.4msec? MotyS
|
8/30/2011 3:32 PM | |
Joined: 7/7/2010 Last visit: 4/26/2024 Posts: 14639 Rating: (2349) |
I can imagine several situations where I want fast precise control with fast low-hysteresis position sensors and not delay unnecessarily for the input state change to be recognized. I can also imagine a saw mill with the majority of the time sawing and minimal time positioning and using the longer filters to let things settle out a bit before resorting to a debouncing TON. Bouncy logs rolling into position. Hope that helps. |
science guy |
|
Follow us on