1/19/2015 3:16 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
It is easier to call FC10 (EQ_STRNG) and simply assign binary address to its output. In case of true status for each global addresses, the base address regarding that comparison can be sent to the output. In this case you have a binary result for each comparison.
Attachment12.zip (132 Downloads) |
1/19/2015 3:21 PM | |
Joined: 12/16/2012 Last visit: 4/24/2024 Posts: 652 Rating: (130) |
FYI (you will have to test it on a PLC)
|
1/19/2015 3:32 PM | |
Joined: 1/28/2009 Last visit: 4/26/2024 Posts: 6838 Rating: (1359)
|
Use Move plus conditions. See the attached file: FC10-->Binary output-->Move a value based binary to target Attachment14.zip (145 Downloads) |
1/19/2015 7:42 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Have attached the code which checks the DESIRED TOOL (DB100) with that of library of tools in (DB200). If match is found then you get the integer value in MW100. If no match is found then a arbitrary value of 501 appears. Just and idea tyou can change it what ever you want in code. No of library tools is currently 100, but you can increase if desired.
AttachmentTool_mat.zip (144 Downloads) |
Last edited by: manmeet at: 1/20/2015 11:18 AMDONE SOME CHANGES IN CODE AND ADDED EXPLANATION. Last edited by: manmeet at: 1/19/2015 7:44 PM |
|
Follow us on