11/9/2021 9:06 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
wait for the approval of you request. this can be up to 2 weeks |
11/9/2021 9:13 AM | |
Joined: 9/6/2021 Last visit: 12/20/2022 Posts: 26 Rating: (0) |
We have a project and l need it today. Could you download it and send me by we transfer? |
11/9/2021 9:16 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
nope, because this is not allowed ! |
11/9/2021 9:17 AM | |
Joined: 9/6/2021 Last visit: 12/20/2022 Posts: 26 Rating: (0) |
In our firm noone is authorized to download. How could l solve this problem? I need it right now |
11/9/2021 9:34 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
create a support request |
11/9/2021 11:21 AM | |
Joined: 3/11/2019 Last visit: 4/26/2024 Posts: 1378 Rating: (244) |
Hi, your firmware offline in project, is older than firmware online on cpu. You don't need a firmwareupdate/downgrade at all. Just ignore the message in download dialog. If you get another message, you can also send a screenshot of the specific message. How do you load the project data if the version of the firmware installed in the S7-1500 CPU cannot be selected in the hardware catalog of your version of STEP 7 (TIA Portal)?
****EDIT**** Also the file you want do download, is an update for the cpu itself. Your cpu is already firmware v2.8. This file is no HSP für update the TIA HW-catalog. maybe this helps regards sancruz |
Last edited by: sancruz at: 11/09/2021 11:23:14Feedback appreciated, please rate |
|
Follow us on