12/10/2014 3:58 PM | |
Joined: 1/17/2007 Last visit: 7/29/2024 Posts: 1544 Rating:
|
One of my colleagues is in the process of porting a S7-400 PCS7 project with ET200M I/O to an S7-1500. All has gone well except for the FM350-2 module. He seems to think that PCS7 to TIA Portal and S7-400 to S7-1500 is maybe too much of a change to perform at one step. So to keep things simple he just tried to port a S7-300 FM350 exmple project (available here http://support.automation.siemens.com/WW/view/en/99742545) to S7-1500. The porting encountered a small number of errors. These are regarding the FM350 interface functions not being supported by the S7-1500 (namely CNT2_CTR, CNT2RDPN, CNT2WRPN & DIAG_RD). So are these functions still needed on the S-1500? If so, what are the new equivalents? Has anyone any experience is interfacing to a ET200M FM350-2 using TIA Portal on the S7-1500? |
Programming today is the race between software engineers building bigger and better idiot proof programs, and the universe producing bigger and better idiots. |
|
10/21/2015 10:05 AM | |
Joined: 11/13/2014 Last visit: 7/18/2024 Posts: 1 Rating:
|
Hi Smiffy, Did you find an solution to use FM350-2 with ET200-M and CPU S7-1500 ? Thank you, Renaud |
Follow us on