5/20/2011 8:29 AM | |
Posts: 241 Rating:
|
can anyone tell me how to disable command of force value in step-7?? Without using feature of security password?? |
5/20/2011 8:53 AM | |
Posts: 691 Rating:
|
Dear Deep Bhatt I think your PLC is password protected, that is why you have to provide password on activating and de-activating the Force Normally it doen't ask any password rather it asks confirmation If you want to remove the Password, then you have to remove from the Hardware Configuration and download it. The CPU will go to Stop mode as you will be downloading the Hardware |
5/20/2011 9:07 AM | |
Posts: 241 Rating:
|
i have password access... but how to totally disable that option..so that non of the user can force the value either by entering pass word.. |
5/20/2011 9:32 AM | |
Joined: 3/21/2006 Last visit: 7/12/2023 Posts: 10221 Rating:
|
Hello, Just change the password with yours. And that's it. You will only know the password after. How can you activate the protection level with a password in the HW Config for an S7 CPU? Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 5/23/2011 4:23 PMCheck it now. Last edited by: UMENCHO at: 5/20/2011 9:33 AMBTW, what kind of CPU do you have there? |
|
5/23/2011 4:18 PM | |
Posts: 241 Rating:
|
i got an error msg while clicking on above link |
5/23/2011 4:24 PM | |
Joined: 3/21/2006 Last visit: 7/12/2023 Posts: 10221 Rating:
|
Check it now. |
5/23/2011 4:27 PM | |
Posts: 241 Rating:
|
without giving password protection is it possible??? |
Follow us on