10/14/2021 2:21 PM | |
Joined: 3/31/2006 Last visit: 4/24/2024 Posts: 39 Rating: (1) |
Hi all, I've installed V17 upd1 and now I'm trying to do my first project with this one. I've used my last project made with V16 as base project, and I'm experiencing some issues with GATHER_BLK function. It seems that the function doesn't accept [0] al first element of the output array ... any ideas? In attachment there is: - V16 original that is working good -V17 converted with compilation error -V17 without error AttachmentGATHER_BLK.zip (110 Downloads) |
Follow us on