8/5/2016 8:44 PM | |
Joined: 12/29/2012 Last visit: 2/6/2024 Posts: 120 Rating: (15) |
Hi to All, I am Using Simotion D410-2 Pn/ DP Controller As a Master and ET200SP, G120 Cu240 E-2, Profinet Encoder As Slaves Of the Simotion . Now I Wants to read the Profinet Communication Status between the Master and Slave. So I Trying to Use the Instruction_getStateOfAllDpStations(). But Now I Received the Function Result Value=16#FFFF8091. & 16#FFFF8090. Details: // Controller – D410 -2 PN/DP Port Used for the Profinet Communication: X150 Software Used: TIA Portal and TIA Scout // Kindly Let Me Know what is the Logical Diagnostic Address to Read the Data from X150 Port Here with I Attached the Screen Shots of the Details Kindly Help Me AttachmentScreen_Shots.zip (213 Downloads) |
Best regards |
|
8/11/2016 12:57 PM | |
Joined: 12/29/2012 Last visit: 2/6/2024 Posts: 120 Rating: (15) |
Hi Christoph, Thanks for your reply, Kindly find the Overall Address List AttachmentSimotion Controller.pdf (233 Downloads) |
Best regards |
|
8/11/2016 8:07 PM | |
Joined: 12/29/2012 Last visit: 2/6/2024 Posts: 120 Rating: (15) |
Hi, Thanks for your reply, Here with i Have Attached my Profinet interface details and my program PDF . Is any Parameter i need to enter in the field of command ID and IoId?. Kindly Let Me know is any error in my Program AttachmentProfinet_Comunication.zip (222 Downloads) |
Last edited by: loga at: 8/11/2016 8:19:04 PMBest regards |
|
8/12/2016 9:00 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980)
|
Hi, you can provide the the project with a external file hoster like dropbox to send the project.
Christoph |
Follow us on