2/6/2012 9:52 AM | |
Posts: 30 Rating: (0) |
Hello friends, AttachmentGSDML-V2_2-SIEMENS-MC-Encoder-20110603 (1).zip (1206 Downloads) |
2/7/2012 2:23 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
Hello, I got the information the file was checked with the XML-Viewer from the PROFIBUS/PROFINET organisation PI (www.profibus.com) without errors. It would be helpfull, if GE could say in which line/object they have problems. |
Last edited by: miami at: 2/29/2012 3:18 PM |
|
This contribution was helpful to1 thankful Users |
2/8/2012 5:20 PM | |
Posts: 30 Rating: (0) |
Hi miami, I will write to GEIP, maybe there is a hiddenissue. Thanks very much! |
2/23/2012 8:57 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
I think you should go in that direction in order to edit existing file. Like an option - Support Request Best regards, Hristo Mihalev |
6/11/2014 3:14 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
Question split toconfigure Mc-encoder 6FX2001-5FN13 with S7-1200. With best regards, Narrator1
|
Follow us on