Industry Online Support
Technical Forum
5/5/2012 6:55 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, I often use SZL W#16#0694: Diagnostic status of the expansion units in the central rack / stations of an IO controller system (Status bit = 1: At least one module of the rack/station is disrupted or deactivated) It works for Profibus and Profinet IO as well. Have a look to that FAQ How do you find out the status of the stations of a DP master system or of a PROFINET IO system?: http://support.automation.siemens.com/WW/view/en/31895566 |
Best regards |
|
This contribution was helpful to1 thankful Users |
Follow us on