6/7/2015 5:56 PM | |
Posts: 7 Rating: (0) |
Hello, I've done the logic part and it's working in LSC (v.8), but when I transfer it to LOGO! (0BA8), it does not work. The problem is caused by an up/down counter which is set to turn on- on 2nd. count and turn off-on 3rd. count. In LSC it works properly but in PLC and online test monitoring it turns on-on first count and turns off-on 2nd. count. The logic is attached for more investigation and that counter is labled B057. after opening attachment, follow instructions below to make it work: Input 1&2 > ON Inp. 3 > ON Inp. 3> OFF Inp. 4&5 > ON Inp. 1&2 > OFF Inp. 3 > ON Inp. 3 > OFF Inp. 4&5 > OFF I'd be thankful if you could help me, and/or give me a suggestion. Nima Attachmenttest_invest_1.rar (209 Downloads) |
Last edited by: Nimasajedi at: 6/7/2015 6:06:22 PMLast edited by: Nimasajedi at: 6/7/2015 6:09:40 PMLast edited by: Nimasajedi at: 6/7/2015 6:17:14 PM |
|
6/7/2015 8:16 PM | |
Joined: 12/18/2014 Last visit: 6/16/2024 Posts: 33199 Rating: (4106) |
Maybe it can be solved so. |
Last edited by: ixo65 at: 6/7/2015 8:52:32 PM |
|
6/7/2015 8:51 PM | |
Posts: 7 Rating: (0) |
Thanks for your reply. I edited your logic as it is attached, but it's not working too. actually the problem is not regarding whole the logic, but only with this counter which is not working in PLC as it should be, even on a simple logic like this one:
And this is the correct movie (also I changed above) : Attachmenttest 1.rar (642 Downloads) |
Last edited by: Nimasajedi at: 6/7/2015 8:54:05 PMLast edited by: Nimasajedi at: 6/7/2015 8:57:38 PMLast edited by: Nimasajedi at: 6/7/2015 8:59:26 PMLast edited by: Nimasajedi at: 6/7/2015 9:01:37 PMLast edited by: Nimasajedi at: 6/7/2015 9:02:00 PMLast edited by: Nimasajedi at: 6/7/2015 9:03:15 PM |
|
6/7/2015 9:06 PM | |
Posts: 7 Rating: (0) |
Could you please check out this one on a PLC if you can see "Hello" word on PLC screen? Thanks Attachmenttest 2.rar (196 Downloads) |
Follow us on