3/29/2016 4:19 PM | |
Posts: 31 Rating: (2) |
Sorry......... What we need is to have the fans to run at a variable speed (100%, 50% and 25%) depending on the temperature and humidity input The fans we are using at the moment are 240v AC and are switched from a thermostat and now need to make the system more efficient I have attached a PDF of the new sensor we are thinking of using Thank you AttachmentHUmidity sensor.pdf (183 Downloads) |
3/30/2016 11:59 AM | |
Posts: 31 Rating: (2) |
thank you again for your input......and patience ! I think we need to rethink the fan control so could we concentrate on the thermocouple side I have attached the PDF of the sensor we are wishing to use and any help with the connection/circuit would be great Thank you AttachmentHUmidity sensor.pdf (133 Downloads) |
3/30/2016 2:18 PM | |
Joined: 12/18/2014 Last visit: 6/9/2024 Posts: 33166 Rating: (4098) |
Here are 2 possible solutions. Solution 1: Solution 2: Solution 1 in attachment, Solution 2 attached at next post. AttachmentFan_Switch_on_off.zip (171 Downloads) |
Follow us on