4/24/2016 9:15 PM | |
Posts: 4 Rating: (0) |
Need help with S602 as a NAT. I am using a SCALANCE S602 V4 and trying to setup as a NAT. It looks like the NAT translation is being done cause I can ping the translated addresses but thats all I can do. I can connect or do anything else with my devices thru the NAT. It looks like it is blocking everything. I have the firewall rule set to be all open and still can do anything else but ping. I have attached my SCT file with one device only where I am testing. My internal subnet is 192.168.0.0, where I have a node 192.168.0.20 Any help would be appreciated AttachmentCD4_Scalance_S602_example.zip (54 Downloads) |
Follow us on