7/31/2022 2:32 PM | |
Joined: 7/28/2022 Last visit: 7/31/2022 Posts: 1 Rating: (0) |
Hello I would be very thankful if somebody can help me with troubleshooting the following issue: My new equipment arrived with probably a faulty motor/decoder or bad configuration resulting in a very loud and annoying high-pitched frequency sound (see the attached video in zip file for sound) the faster the motor goes - the louder the sound. The motor is 1FL6042-2AF21-1AG1 (connected to v90), the configuration file from the v-assistant is attached in the zip file. I am also encountering alarm A1932 but I don't think it's related Looking forward to any of your suggestions (FYI I am coming from a totally different tech domain and its the first time I am dealing with PICs so explanations can be very helpful here) Thanks! Attachmentnoise_files.zip (409 Downloads) |
8/5/2022 2:20 PM | |
Joined: 12/16/2021 Last visit: 8/22/2023 Posts: 126 Rating: (1) |
Hi NadavL At what speed this noise issues occurs ? May be at lower speed this can be resolve. Regards
|
If The Information Helpful, Then Don't Forget Give (To thank ) and Rate It |
|
Follow us on