1/23/2010 1:49 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835)
|
Hello, Your question belongs us to the differences between incremental and absolute encoders. The differences have been discussed in this thread. And after reading the above thread link, I think if you would like to keep the position of the shaft although if the power switched off, then you have to use absolute encoder. And keep in mind if you changed your sellection from incremental to absolute encoder, this will have a reflection on the sellection of FM which reads the encoder signal. Or you can select profibus absolute encoder. Regards, |
Ayman Elotaify |
|
1/23/2010 4:49 PM | |
Posts: 23 Rating: (0) |
thank u |
1/23/2010 7:15 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at Remanent data areas of the S7-22x and Duration of the Retentive Feature in S7-21x and S7-22x Hope this helps. best regards, Hristo Mihalev |
1/25/2010 8:52 AM | |
Posts: 37 Rating: (2) |
Hi AttachmentSnaps.zip (139 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on