9/7/2020 12:33 AM | |
Posts: 2 Rating: (0) |
Hello, I have a problem with the historical data with WinCC Advanced V15 on Windows 7 Professional. I have configured the data logs and alarm log, I have verified that the files were created and populated with data, but both the trend view and the alarm view show nothing at all. You can see pictures with the actual config in the attached ZIP. Figure_1: Alarm Logs config Figure_2: AlarmView config Figure_3: File with alarm log info opened with notepad Figure_4: Empty historical AlarmView in runtime Best regards. AttachmentFigures.zip (65 Downloads) |
Last edited by: Fredd_eproc at: 09/09/2020 14:11:34 |
|
9/11/2020 8:19 AM | |
Joined: 8/3/2009 Last visit: 4/30/2024 Posts: 12869 Rating: (1643)
|
Hello Fredd_eproc I have found also this FAQ to this Topic What can you do if no alarm log is displayed in the Alarm View at runtime, but the logging of alarms still works? https://support.industry.siemens.com/cs/de/en/view/109778759 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on