4/14/2009 1:31 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear gendy, Here is a link to Catalog ST80: http://www.automation.siemens.com/salesmaterial-as/catalog/en/st80_e.pdf you can choose a panel to communicate with S7-300 using MPI or Profibus (both RS485) Example: TP177A (but the choice depends on what you want ) When you use a non-siemens panel, you need driver to communicate with S7-300. Best regards, Wizard |
4/14/2009 3:04 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello gendy, You could look at EXOR's UniOP family of HMI panels. I am using this this type panel, connected via Profibus... If you need more information, let me know... Hope this will helps. Best regards Hristo Mihalev |
4/19/2009 6:59 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello gendy, It is not possible someone to show you all panel's brands that support Profibus. And you are right, all of then use external Profibus card. And this cards is made by the same company. This is normal, becouse PROFIBUS (Process Field Bus) is a standard for field bus communication in automation technology. In this way manufactories made their panel more "flexible" and useful with more possibilities. About brands, I suggest you try to search in google for it. I found this ones: - EXTER; - Telemecanique Magelis XBT GT; Best regards Hristo Mihalev |
Follow us on