5/27/2012 11:22 PM | |
Joined: 5/28/2008 Last visit: 12/5/2023 Posts: 4486 Rating:
|
Hello, That's true. New version of BW500 accepts up to three belt scale load cells (i.e. 6 load cells). It goes without saying that all belt scales should be attached to the same belt conveyor. In this manual "Milltronics BW500 - Instruction Manual", in page 18, the connection of 6 load cells. It's clear that three load cells are connected in parallel to load cell A input, and the other three load cells are connected in parallel to load cell B input. load cell C & D inputs are bridged with A & B. In page 112, please read how to enter the number of load cells to BW500. For both 4 or 6 load cells, enter number 4 in P003 (No. of load cells). Hope this helps.
|
Last edited by: Ayman Elotaify at: 5/27/2012 11:25 PMLast edited by: Ayman Elotaify at: 5/27/2012 11:23 PMAyman Elotaify |
|
Follow us on