12/18/2017 7:34 AM | |
Posts: 16 Rating: (1) |
Dear experts I want to create a face plate in pcs7 version 8.2, but there is not any face plate manager in this version of PCS7. I have worked with 7.1 and I know that it has a face plate manager, it which the user will be able to manage and create face plates corresponding to self created blocks in the logic. So by using this face plate manager I was able to connect inputs/outputs my created blocks to a faceplate also I was able to create faceplates' pages. I wan to know how I can create a faceplate while I can not find any faceplate manager in the Wincc software. I would be grateful if you guide me in this issue. Sincerely ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/18/2017 12:33:21 PMNew subject after splitting |
|
12/18/2017 1:39 PM | |
Joined: 4/8/2016 Last visit: 5/21/2024 Posts: 133 Rating: (45) |
Hey saharahmadzadeh, firstly I wouldn't recommend to create own faceplates since it's quite a lot of work. But if it is required it is possible. The faceplate designer you were looking for isn't included in the standard installation anymore. If you want to use it, you can install it on your own, the following post should help you: https://support.industry.siemens.com/tf/ww/en/posts/pcs-7-v8-0-where-can-i-find-the-faceplate-designer/77282/?page=0&pageSize=10 But do you want to create a faceplate in conformance with APL? If yes, you should have a look at the APL Style Guide, as there is no designer for faceplates in conformance with APL: https://support.industry.siemens.com/cs/ww/en/view/65601446 |
Kind regards |
|
Follow us on