11/24/2022 11:32 PM | |
Joined: 4/28/2015 Last visit: 8/20/2024 Posts: 36 Rating: (0) |
How can I download UC01 or UC02 (preferable) now? ------------------------------------------------------------------------------------------ |
Last edited by: RoVRy at: 11/25/2022 00:11:59Last edited by: Jen_Moderator at: 11/25/2022 11:57:43New subject after splitting |
|
11/25/2022 9:03 AM | |
Joined: 10/26/2011 Last visit: 9/9/2024 Posts: 762 Rating: (191)
|
Hello, Only the latest Update Collection will be provided, as is usual when ordering PCS 7. Here you will also always receive only the PCS 7 version with the latest service pack. It is recommended to install the latest update collection of the PCS 7 version. |
SIMATIC PCS 7 - Overview |
|
11/25/2022 10:23 AM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi, Since V9.0 Siemens has changed the software update section a bit, also with the addition of Update Collections. But in the software update section, you can see the separate components and behind them is a small number indicating it's included in UC01, 02, 03 etc. So, you can download the updates separately and install them separately, but please use the compatibility tool to check which is compatible with each other. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on