1/26/2022 2:28 PM | |
Joined: 8/3/2009 Last visit: 6/4/2024 Posts: 12991 Rating: (1655)
|
Hello As I wrote you can define the style hardcoded inside the Faceplate as string. (the same is also documented in the help system) But will see the "result" only in the faceplate instance, not in the definition. https://support.industry.siemens.com/cs/ww/en/view/109773506/69428166283 "..... Support of styles in faceplatesStyles and style items can be assigned to faceplate instances. However, there is no direct connection between the faceplate types and styles, so selection and preview of a style item in the faceplate editor is not possible. To assign a style item to a faceplate, enter the name of the style item under "Style item appearance". The configured style item is used in the instance of a faceplate, provided the name of the style item exists in the style used. Ensure that the name is written correctly. ...." Bye Murof |
Last edited by: Murof at: 01/26/2022 14:32:25If this Information really helps, you could use the Rate function |
|
Follow us on