1/12/2012 2:28 PM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190) |
How can I convert a dynamic dialog to an on event action? Problem Due to the inefficiencies inherent to Dynamic Dialogs during Runtime it is strongly encouraged to avoid them. Since it is simple to convert a Dynamic Dialog to a script this is a good start, however, having this script executed every few seconds is unnecessary. Instead, it is possible to setup the object so that the script is only called when needed. This is what will be explained in this document. Solution See attached (text too long). AttachmentConfiguration_Steps.pdf (69 Downloads) |
SIMATIC PCS 7 - Overview |
|
1/13/2012 1:57 PM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
Maybe you can share a example of a dynamic dialog useage whith bad performance then I can see what you mean. |
Follow us on