9/13/2017 8:48 AM | |
Posts: 20 Rating:
|
Hi i am using the IOT2000 IO module on the IOT2040.I need to control a motor using PWM .The manual for the IOT2000 IO module says that D9,D10 and D11 maps to digital inputs DI3,DI2 and DI1 on the IO module .PWM is possible on D9,D10 and D11 as per the IOT2000 operating instruction manual .How is PWM possible on the digital inputs? Regards, Mathew ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/14/2017 10:03:05 AMInserted splitting-remark. |
|
9/13/2017 9:22 AM | |
Posts: 20 Rating:
|
Hi , I understand that PWM is possible on D9,D10 and D11 pins ,but In the IO module these pins are designated as Inputs so how can i get a PWM signal on the Input.In Node red the intel_gpio node also has a PWM option which acts as an output node but since D9,D10 and D11 are inputs i am not able to do the PWM through the IO module. Help much appreciated. Kind Regards, Mathew ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/14/2017 9:58:49 AMNew subject after splitting |
|
Follow us on