5/29/2019 9:58 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983) |
hi, from the s7bas is it Winccflexible 2008 SP3 downloadlink: https://support.industry.siemens.com/cs/ww/en/view/100777999 you need the Compact/standard/advanced is not relevant whether you modify the panels or not. You open and work with a project which contains WinCCflex components. So the missing SW package pops up and tell you that. you can ignore this message , but as you see the project can not really used without the needed SW Package. you can also make a "Save as" with the option reorganize. then some parts of the project are removed for which no packages are installed, but then you have a project with some other content like the one have on the machines, but you get no message for missing SW :) .
Christoph |
This contribution was helpful to1 thankful Users |
5/29/2019 2:59 PM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Thank you again ChristophD, Please see the new screenshots. I installed the Winccflexible 2008 SP3 and did another HW update electing to install all the possible updates. At least I no longer get a warning for missing WinCC Flex SW. I did however get a rather long list of failed updates and I am still getting a warning for missing or outdated HW software and many nodes are missing in the HW configuration image. If it helps I can also attach a screenshot from an ES (with newer Step 7 and WinCC versions where all the HW nodes are present?
AttachmentHW error.zip (120 Downloads) |
Follow us on