5/27/2019 10:53 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Please also see the screenshots. We are running on older SW on some of our machines. I need to install an Engineering Station to work with these machines. The WinCC in version 7.0 SP3 Upd.1. I have been told on this forum that the newest Step 7 I can use on integrated projects with this WinCC is version 5.5 SP 2 so I have installed this. I have also installed the S7 safety pack we have available. But after installing the various packages I am still getting some faults for missing updates/outdated versions. How do I get to know exactly what I need to install and are the missing updates etc. downloadable from the Siemens page? I tried running the the execute file under the "Required Software Packages"but it did not produce any additional information. Please see the screenshots for installed SW and fault messages etc. AttachmentDiv1.zip (153 Downloads) |
5/28/2019 9:21 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hello ChristophD, Thank you for a very useful answer. I cannot see the safety modules in the version files - or how can I search for their versions? Below is an example (file also attached) - can you tell me the correct version of Step 7 from this? [snip]
AttachmentStep7Bas.zip (155 Downloads) |
Last edited by: Jen_Moderator at: 05/28/2019 09:35:39Removed example and inserted it in a txt file and moved it to the ZIP file, because it was too long. |
|
5/29/2019 9:14 AM | |
Joined: 9/30/2016 Last visit: 4/5/2024 Posts: 910 Rating: (6) |
Hi again ChristophD, Please also see the attached screenshots. We are getting closer bit by bit. I DL'ed installed the the missing SP13 for the safety SW and I DL'ed and installed all the HW updates that was available to DL and possible to install. Now the Safety SW got the right SP and there is not longer a warning for missing weight cell software. And as mentioned previously we will disregard the missing support for the Flex panels. There is however still a warning for missing or outdated HW software and many nodes are missing in the HW configuration image. So how do get the last missing / outdated SW in the right order?
AttachmentHW.zip (141 Downloads) |
Follow us on