1/9/2006 6:26 PM | |
Posts: 4 Rating:
|
I am trying to update the hardware catalogfor Step 7 version 5.1to include the 6GK7 343-1EX110OXE0. How do I do this? |
1/10/2006 10:28 AM | |
Joined: 8/31/2005 Last visit: 5/16/2024 Posts: 217 Rating:
|
Hi Rick! A GSD file is a device database, which contains all properties of a DP-slave. GSD files are provided by the manufacturer of the device. But you are looking for the CP 343-1 - for this device there is no GSD file. I think you should try to install SP6 for STEP 7 V5.1 (download via this link: http://support.automation.siemens.com/WW/view/en/12642848). For STEP 7 V5.1 this is the only possibility to update the hardware catalog. STEP 7 since version 5.2 supports the download of hardware updates from the internet (see also this FAQ: http://support.automation.siemens.com/WW/view/en/22306445). |
Greetings, Chris |
|
Follow us on