4/5/2012 2:13 PM | |
Posts: 30 Rating:
|
Thanks again for you aresaving me. S7 have to be conected to new printer. I am planing to order a CP340, RS232 C (6ES7340-1AH02-0AE0), mount it next to CPU, and contect it with serial buss to priner. It must be an "old fashion matrix printer". Do not ask my why S5 application contain 5 DB:s. It´s DB1, DB6, DB100, DB206 and DB255. As you told me before, DB1 contain specifc S5 information, that is not nesecery for S7. So in DB1 can "text" not be hiding? DB6 and DB 206 isautomaticgenerated from OB 21 , ( S7 OB101 - Hot restart) A F 1.0; R F 1.0; //RLO "0" AN F 1.1; S F 1.1; //RLO "1" ; L KF +255; G DB 6; G DB 206; : JC PB 6 //Fault text OB21/OB22 so text should not be hiden in to DB 6 and/or DB 206 either!?! So what I still got is DB100 and DB206. DB100 But I can not find anything as Text into them? But there is a file, in project, called *.525 .Is that "text" file? And how to open it? All files in project are following: APP File APP 525-file APP@@F1 APP@@F2 APP@@PJ APP@@ST.S5D S5D-file APP@@XR APP@@Z0 APP@@Z0.SEQSEQ-file APP@@Z1 APP@@Z2 APP@@ZF.SEQSEQ-file |
Last edited by: Nisse11 at: 4/5/2012 3:03 PM |
|
4/5/2012 9:32 PM | |
Joined: 7/18/2011 Last visit: 10/9/2023 Posts: 521 Rating:
|
Hello Nisse11, I think you'll find a lot of usefull information in this COM 525 manual. Take especially a look at chapter 7 (page 131/534) about Sequential Messages. Kind regards, BV |
4/10/2012 4:15 PM | |
Posts: 30 Rating:
|
Great and THANKS A LOT!!!![]() So, ifI understaind it right , that would be, for example: - Alarmtext nr 0001 ( Utl. Linje Skydd K2 ) is setting by FW156, F 156.0 ? (since F 156.0 isfirst bit, nr.1 in FW156?) and -Alarmtext nr 030 ( Utl- Dvärgbrytare SRR2) is setting by FW158, F 159.5 ? (since F159.5 is bit nr.14 in FW 158?) and so on...? If its like that above I write, then I now understaind how its work. Next thing will be how to do (allmost) same thing in S7, but I guess this manual explain it rather well for me. Im am planning to use Cp340, so this should be right: https://support.automation.siemens.com/WW/llisapi.dll?query=cp340+print&func=cslib.cssearch&content=adsearch%2Fadsearch.aspx%3Ftab%3D2&lang=en&siteid=csius&objaction=cssearch&searchinprim=_searchinprim_&nodeid=99&x=16&y=8&cssearchengine=NEW |
Follow us on