9/26/2022 7:36 AM | |
Joined: 2/17/2019 Last visit: 8/21/2024 Posts: 3 Rating: (0) |
Hello , How much connection can i add in Wincc Advanced because i am getting issue. I have Tia Portal Wincc 17 Advanced it is show Wincc Advanced -Properties-Connection resouces. it is showing only 2 connection i want to increase how can i increase sir. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/26/2022 11:51:52New subject after splitting |
|
9/26/2022 2:43 PM | |
Joined: 5/30/2022 Last visit: 9/20/2024 Posts: 581 Rating: (96) |
Hi mukesh251296, The number you highlight in the image means the following: "Maximum number of used PLC resources per HMI connection. This parameter is a factor that is to be multiplied by the number of HMI connections used offline. The product is the number of HMI resources occupied on the CPU." In short, the number of PLC resources consumed by each HMI connection. You can find this information in the manual: Display of connection resources |
If this information really helps, you could use the Rate function. |
|
Follow us on