10/11/2017 8:09 AM | |
Joined: 6/27/2017 Last visit: 7/23/2024 Posts: 24 Rating: (0) |
hi, how to communicate hmi and plc in tia14 using simulation mode. Plc used: s7 1200 1212c dc/dc/dc HMI: kp 1200 comfort. we tried with following methods but cant able to create communication. 1. we tried with Pg/Pc interface with s7 online->PLCSIM TCP/IP. 2. PLC got downloaded in simulation mode and when we put in a simulation it went to simulation but the thing is that it wont communicate with PLC. It shows like ##### in the screen. 3.After that we tried with Real PLC S7 1212c we made a PG/PC settings correctly. PLC got downloaded with real PLC after that we put HMI in simulation it went to a simulation but again it shows like the ###### in the screen. Please help us to establish communication between PLC and HMI. ------------------------------------------------------------------------------------------ |
Last edited by: sharfras at: 10/11/2017 8:10:50 AMLast edited by: Jen_Moderator at: 10/12/2017 8:39:49 AMNew subject after splitting |
|
10/12/2017 10:03 AM | |
Joined: 8/3/2009 Last visit: 8/6/2024 Posts: 13467 Rating: (1704)
|
Hello sharfras two things you have to check: - Look in the Connections Editor of your HMI Panel-> in the middle Screen you can see the Access Point of the Ethernet Connection. As default there should be S7ONLINE if you have something else here like S7ONLINE1 or something then it won´t work until you change it to default or you create this Access Point in PGPC Interface settings - https://support.industry.siemens.com/cs/de/en/view/109742764 (- and of course you should check all the basics like security Settings of the PLC, visible Attributes in the DBs and so on ...) Bye Murof |
If this Information really helps, you could use the Rate function |
|
1/15/2018 4:55 PM | |
Joined: 5/3/2012 Last visit: 6/23/2024 Posts: 161 Rating: (2) |
Second: connection Plc to hmi. |
Last edited by: David1981 at: 1/15/2018 4:56:14 PM |
|
Follow us on