11/27/2020 10:56 AM | |
Joined: 3/14/2013 Last visit: 5/15/2023 Posts: 3 Rating: (0) |
In the similar lines, Can anyone tell me , how to configure Master Class 2 in PCS 7? Is it that we have to do at Hardware configuration? what else is required apart from configuration to pull the data. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/27/2020 12:45:27New subject after splitting |
|
12/3/2020 11:38 AM | |
Posts: 198 Rating: (60) |
Hello, I do not think the procedure to configure Master Class 2 in PCS7 is very different from what we could do with PC Based Automation systems. (Using a PC with CP5613 & SIMATIC NET installed, OPC Scout as OPC Client and the relevant configurations in HW Configuration for the same.) Which version of PCS7 are you using? There is a FAQ (quite old) which explains the procedure of configuring an OPC Server with CP5611 in the HW Configuration and creating a S7 connection for the same. https://support.industry.siemens.com/cs/us/en/view/15364951 There is some general information about the OPC Server for Profibus which might interest you too: https://mall.industry.siemens.com/mall/en/in/Catalog/Products/9300160?tree=CatalogTree |
Last edited by: Jen_Moderator at: 12/03/2020 12:48:49Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on