8/29/2022 4:00 AM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150)
|
Hello, Application, version and configuration: Maintenance Station focuses on "Plant Asset Management" and enables preventive and predictive diagnostics and maintenance of the plant. In parallel with process control, the Maintenance Station makes available consistent maintenance information and functions for the system components (assets). While the plant operator receives all process-relevant information and can intervene selectively in the process via the operator system (OS), the maintenance engineer inspects the automation system hardware and processes the associated diagnostic messages and maintenance demands via the Maintenance Station. The basis for a Maintenance Station is always an OS that provides this maintenance functionality. The below linked manual will help you in configuring the Maintenance Station (MS) SIMATIC Process Control System PCS 7 Maintenance Station V9.1 SP1 Section 5 - Configuring the maintenance station will guide you through configuration. |
This contribution was helpful to1 thankful Users |
Follow us on