6/29/2021 11:55 AM | |
Posts: 1 Rating: (0) |
Hi everyone! I am currently working in a project where I have to use one LOGO8 - 6ED1052-1HB08-0BA0, and I have to use another expand card module 6ED1055-1CB10-0BA2. I could not find any information about how I will connect this 2 modules together, and how I will address the I/O located on the expanded module on the logo software. If someone could help me, thanks in advance. Misael Alves Mendes ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/29/2021 14:50:47New subject after splitting |
|
6/29/2021 12:51 PM | |
Joined: 12/18/2014 Last visit: 6/4/2024 Posts: 33147 Rating: (4095)
|
The modules are flanged to the right side of the left module. First remove the cover cap for the contact slide from the respective left module and then slide the contact slide to the left until it clicks into place. AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 36.pdf (288 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on