8/1/2018 9:26 PM | |
Posts: 85 Rating: (0) |
Hello, I want to connect WinCC V7.4 to a PERAX PLC. So I can read tags from the PLC and put them in a SCADA system. Any idea to begin with this PLC... Many thanks |
8/2/2018 12:34 AM | |
Joined: 9/19/2009 Last visit: 5/11/2024 Posts: 458 Rating: (82) |
Hi The only choice you have is check if this PLC have any OPC Server. You can check with KepServer or Matrikon. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
This contribution was helpful to1 thankful Users |
8/3/2018 4:48 PM | |
Joined: 9/27/2006 Last visit: 5/18/2024 Posts: 12257 Rating: (2668) |
Hello CMI Impianti; Have a look here: WinCC v7.4: Communication https://support.industry.siemens.com/cs/co/en/view/109736225 Hope this helps, Daniel Chartier |
This contribution was helpful to1 thankful Users |
Follow us on