4/21/2016 8:12 AM | |
Posts: 35 Rating: (1) |
I now have to create a Tia project from scratch with alarm handling etc. Is there some templates or how do i begin ? I have only worked with PCS7 and wincc before. The project will contain 3 frequencyconverter pumps, and several temperature regulators. The op panel should also be connected to s7 classic (device plc proxy). Maybe there is a guide or demo project to help me getting started ? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 4/21/2016 9:21:56 AMNew subject after splitting |
|
4/21/2016 8:14 AM | |
Joined: 8/14/2014 Last visit: 4/5/2024 Posts: 144 Rating: (17) |
If you have old wincc project from your client, you can import it to TIAp |
4/26/2016 5:47 PM | |
Posts: 35 Rating: (1) |
No I have not, I need to create one from scratch. Is there a manual in english for beginners ? |
4/26/2016 7:23 PM | |
Joined: 3/28/2015 Last visit: 5/4/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: 1-Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x |
Eng.Mohamed Ibrahim |
|
4/26/2016 7:36 PM | |
Joined: 9/22/2014 Last visit: 1/8/2024 Posts: 89 Rating: (13) |
hello, I think this might help : https://support.industry.siemens.com/cs/ww/en/view/54430386
Thanks, Pratts23. |
Last edited by: The Helping Hand at: 4/27/2016 9:49:49 AMMade the first link clickable and replaced the second link by a static one |
|
Follow us on