3/6/2020 12:54 PM | |
Joined: 4/24/2006 Last visit: 6/5/2024 Posts: 8672 Rating: (1158) |
Hello, Have you seen this link: Best regards, Wizard |
3/6/2020 12:59 PM | |
Joined: 10/22/2019 Last visit: 5/29/2024 Posts: 5 Rating: (0) |
Hello, Yes, I have read this and it's still giving me an error message. BAR |
3/6/2020 1:40 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051)
|
hi BAR_BASS, first: download is loading to PLC and upload is loading from PLC To Upload the project see the FAQ, that is mentioned. It is possible to upload. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?also see the other FAQs, that are mentioned there. When you want to change something and load that changes to the PLC, you first need to upgrade the project to a V16 project and load the complete V16 project to the PLC. regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
3/6/2020 1:44 PM | |
Joined: 10/22/2019 Last visit: 5/29/2024 Posts: 5 Rating: (0) |
Thx |
Last edited by: BAR_BASS at: 03/06/2020 21:55:53 |
|
Follow us on