12/3/2022 11:56 AM | |
Joined: 3/18/2020 Last visit: 5/29/2024 Posts: 4 Rating:
|
Hi. I have task to migrate S7-300 system to S7-1500. HW configuration includes CPU 315-2 DP with two ET200B modules (6ES7 131-0BL00-0XB0) and some other devices on Profibus. In Step 7 program which is uploaded from S7-300 PLC can be seen that ET200B modules are configured with GSD file: SI0004AX.200. This migration will be done in two steps. In first step I will replace just CPU with ET200SP and other devices will be retained. In second step, one by one Profibus devices will be replaced. Here I have two questions if anyone can help. First one, is it possible to get this x.200 gsd file somehow in order to make migration to TIA portal with hardware configuration included. I have searched web for this gsd but without success. [snip] Best rregards. tomo314 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/05/2022 08:59:58New subject after splitting. Division of questions into separate topics. |
|
12/5/2022 8:58 AM | |
Joined: 6/19/2017 Last visit: 6/26/2024 Posts: 8183 Rating:
|
New question published by tomo314 is split to a separate thread with the subject Can make migration from Step 7 to TIA Portal without hardware configuration migration?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on