5/27/2019 10:31 AM | |
Joined: 5/22/2019 Last visit: 11/28/2023 Posts: 43 Rating: (0) |
I need to import instead of export user alarms (but the principle is the same) and I'd like to automate it through openness: I already wrote a program that extracts the alarms from a step7 project and creates an xlsx file to import, currently the import process is manual and considering there are 10 HMIs in the project it's cumbersome and error prone. I'm using ironpython instead of C# so I can interactively explore the attributes of the project and its various components. I got to the HmiTarget but there I only see the attributes listed in the diagram (Connections, Cycles, GraphicLists, ScreenFolder, ScreenGlobalElements, ScreenOverview, ScreenPopupFolder, ScreenSlideinFolder, ScreenTemplateFolder, TagFolder, TextLists, VBScriptFolder). I cannot find anything related to the alarms. I cannot believe Siemens left out the alarms! (actually that was tongue in cheek ) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2019 08:46:33New subject after splitting |
|
6/25/2020 11:28 AM | |
Joined: 11/7/2018 Last visit: 5/30/2024 Posts: 1 Rating: (0) |
i have the same problem. How to find the alarms? any news? |
Last edited by: Dan1424 at: 06/25/2020 11:50:52 |
|
Follow us on