3/20/2019 10:20 AM | |
Joined: 3/27/2017 Last visit: 8/22/2024 Posts: 11 Rating:
|
Dear all Moderator 4rum, I have 01 Sinamics Compact Flash Card 6SL3054-0ED01-1BA0 w Per. 4.3.1 and I insert to CU320-2PN, firmware not compatible ( CU320-PN SUPPORT FROM V4.4 OR higher) when i read this Instructions manual and follow it, Cu320-PN light is Orange light. If i insert CompactFlash card to CU320-DP, light is on Green, not Flash 2s. All two case, Scout not found CU on Access node? If I use TIA V13, it found MAC ADDRESS: 00-1F-F8-24-B7-EE but not found IP Address. How to update firmware to V4.4, V4.5 OR V4.8 and fix it? CU320-DP: 6SL3040-1MA00-0AA0 CU320-PN: 6SL3040-1MA01-0AA0 Thank you very much! AttachmentInstructions_Firmware_Update_S120_08_2016_CU310_2_CU320_2.pdf (545 Downloads) |
Last edited by: TruongVu at: 3/20/2019 10:23:04 AMTruongVu |
|
3/20/2019 10:44 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
Hello, and if you then set a ip on this found device is it working or not? Christoph |
3/20/2019 11:04 AM | |
Joined: 5/12/2006 Last visit: 9/3/2024 Posts: 22352 Rating:
|
do you have this on both cu? Do you have delete the USER Folder? Christoph |
Follow us on