Industry Online Support
Technical Forum
4/10/2014 9:25 PM | |
Posts: 67 Rating: (5) |
Hello, I use NetPro to connect the network from X127 and X150, I add a PG in the project. I made a hardcopy from netpro that could help. I configure CU320 in Starter commissioning interface to set ip address to X150 Pierre AttachmentNetPro_CU320.pdf (290 Downloads) |
This contribution was helpful to1 thankful Users |
4/16/2014 11:31 AM | |
Posts: 13 Rating: (0) |
Thanks, it's work. I also add a PC/PG in network and I directly upload the program though STARTER software |
Follow us on