Industry Online Support
Technical Forum
3/22/2011 12:09 PM | |
Posts: 40 Rating: (1) |
Hi ocuaxanh, As far as I know there are no loops available in S71200 as of now. When V11 of Step-7 basic comes with SCL then you will be to use for loops. So if you can't wait then design a logic or repeat the compare logic with different variables for 30 times. |
3/28/2011 3:57 PM | |
Posts: 10 Rating: (0) |
Dearhuggy_d1, Thanks for your susggestion. May you send me these kinds of links? Thank you, Ocuaxanh
|
3/28/2011 5:33 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15204 Rating: (2417) |
The S7-1200FAQs appear for me at this link : https://support.automation.siemens.com/US/llisapi.dll?func=cslib.csinfo&objid=48815048&caller=view The help file available in the S7-1200 TIA Portal V10.5 software, click the help (or press F1) menu option. From there, you will find the same information that is also available online: https://www.automation.siemens.com/mdm/default.aspx?Language=en&GuiLanguage=en&DocVersionID=19532831883&TopicID=15105542411&Highlight=&Query=&cssearchengine=NEW Your links may appear differently once you set the location and language. I found the TIA Portal help files to work fairly well. I exceeded the watchdog timeout several times while developing the first loop, so be prepared for a PLC STOP during your loop implementation. I also posted a few forums items which include links. The forums allow you to search forum posts by specific users. May be helpful to check out that and the Pegaia tips for S7-1200. |
science guy |
|
Follow us on