9/8/2011 9:02 AM | |
Posts: 4 Rating: (0) |
Hi, I have W7 prof with XP virtual mode and Step7 5.5 (Step7 Prof 2010). Under W7 I can't install Scout Simotion, so I've installed Step7 with Scout Simotion to XP virtual mode. The Simatic USB MPI (DP) adaptor is installed OK (when i connect the adapter , I see that the Simatic PC Adapter is connected ), but I can't find in Step7 - Options - Set PG/PC Interfaces the PC Adapter Profibus. Do you have any suggestions Thanks Martin Splitted from USB MPI adaptor for S7 300 in virtual mode. |
Last edited by: O_Moderator at: 9/8/2011 9:25 AMnew subject after splitting |
|
9/8/2011 9:09 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello Martin, Take a look at How do you assign the parameters of the PG/PC interface in general and what is the remedy if the device driver cannot be selected or is not visible? best regards, Hristo MIhalev |
9/8/2011 2:50 PM | |
Posts: 4 Rating: (0) |
Hello, solved by Add/Remove. Thanks a lot |
This contribution was helpful to1 thankful Users |
Follow us on