3/1/2021 11:47 AM | |
Posts: 40 Rating:
|
and screenshot of HMI: |
3/1/2021 11:51 AM | |
Joined: 6/10/2015 Last visit: 8/21/2024 Posts: 468 Rating:
|
You can't upload HMI (upload: from the target to your computer) |
B. Edulis |
|
3/1/2021 11:54 AM | |
Posts: 40 Rating:
|
yeah you are right, what does it mean? I dont have access? |
3/2/2021 11:18 AM | |
Joined: 3/11/2019 Last visit: 9/6/2024 Posts: 1569 Rating:
|
Dear zuzwha, please check the online & diagnostics of the cpu. There you can find the version of TIA the CPU was configured with (please find also screenshot attached). This filed is only filled, if the cpu was configured with TIA V14 or newer. If the field is empty, the CPU was configured with an older version. In general, the version the CPU was downloaded with, must be known. Please also check the following FAQ according compatibility and use the compatible version of TIA. What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC?regards sancruz #############EDIT################ Upload is only possible from CPU, not from HMI |
Last edited by: sancruz at: 03/02/2021 11:20:36Feedback appreciated, please rate |
|
This contribution was helpful to
2 thankful Users |
Follow us on